Technical FAQs

Ask a Question

Are the ATV21 and ATV212 drives plenum rated?

The open type ATV21/ATV212 and the enclosed SFLEX are plenum rated. The SFLEX is stated in the brochure (8839BR0501R8/07) under environmental specs and also in the SFLEX Instruction Bulletin (30072-451-83C).

CTA-ID : 2050860
Was this helpful?
What can we do to improve the information ?