Technical FAQs

Ask a Question

What is the current rating for a PKxxGTA Equipment Ground Bar?

Equipment ground bars are not current rated as they are not a current carrying component.




Issue:
Are PK**GTA ground bars current rated?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker load centers and panelboards sold and supported in the USA.

Cause:
Current rating on ground bars.

Resolution:
Equipment ground bars are not current rated as they are not a current carrying component.



CTA-ID : 2050856
Was this helpful?
What can we do to improve the information ?