Technical FAQs

Ask a Question

How many lugs can be put on a RG 3000a 100% rated breaker?

The RL3TB terminal pad kit can handle 9 lugs per phase connection. They must be installed in pairs with one by itself . Mechanical lug kit # AL2500RK consists of 2 lugs and has a wire range of 1/0 AWG to 750 kcmil.

CTA-ID : 2050168
Was this helpful?
What can we do to improve the information ?