Technical FAQs

Ask a Question

What could be wrong if the HVL/cc field shaper is somewhat loose and the bolts holding it are tight?

The bolt is too long and should be replaced with a shorter one.

CTA-ID : 2050965
Was this helpful?
What can we do to improve the information ?