Technical FAQs

Ask a Question

Are there any application limitations when using a L400LS circuit breaker enclosure?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Application

Resolution:
Yes, the LA400LS has application limitations. The LA4000LS is UL listed only to accept a LAL, 3-Pole circuit breaker. The voltage is limited to 480Vac maximum. The SCCR is limited to 30K rms symmetrical amperes at 480Vac maximum. Copper conductors must be used (aluminum conductors are not acceptable).


CTA-ID : 2050781
Was this helpful?
What can we do to improve the information ?