Technical FAQs

Ask a Question

Are there any application limitations when using a JD250S circuit breaker enclosure?

Issue:
Product design limitations

Product Line:
Circuit Breaker Enclosures

Environment:
Product limitations

Cause:
Application

Resolution:
Yes, the JD250S Series A01 is UL listed ONLY to accept a HDL or JDL, 3-Pole, 80% rated circuit breakers. The voltage is limited to 480Vac maximum. The SCCR is limited to 18K rms symmetrical amperes at 240Vac or 480Vac. Copper conductors(75 degree C) MUST be used (aluminum conductors are not acceptable).


CTA-ID : 2050778
Was this helpful?
What can we do to improve the information ?