Technical FAQs

Ask a Question

Can double barrel lugs be used on the 400 amp Powerpact DGP36400E20 breaker?

Yes, the 600 amp lug kit for one side (cat. # 32510) will work with the 400 amp breaker. Wire range (2) 2/0-350kcmil Cu; (2) 2/0-500kcmil Al.

CTA-ID : 2050767
Was this helpful?
What can we do to improve the information ?