Technical FAQs

Ask a Question

What are the replacement parts for UFP222RD, Series G02, AC Disconnect?

Only the parts listed below are considered field replaceable (for pictures see attached link):
Only the parts listed below are considered field replaceable (for pictures see attached link):
Interior Trim - Cannot be provided due to UL labeling issues.
Pullout - 4050711750 (This pullout will work for either Series G01 or G02)
Interior Trim Mounting Screw  4020513001K (This kit includes 10 screws. Only one screw is required)
Receptacle - Purchase locally, Leviton #BR20-GY or equivalent (NEMA 5-20R, 125V, 20A, 2 Pole, 3 Wire Grounding, Duplex)
Receptacle Mounting Screws (2) - Purchase locally, 6-32 x .375 Machine Screw
Receptacle Mounting Nuts (2) - Purchase locally, 6-32 Hex Nut


CTA-ID : 2050765
Was this helpful?
What can we do to improve the information ?