Technical FAQs

Ask a Question

Is there a 200A Main Breaker for a HOM2040L200TC (main lugs) load center?

If the HOM2040L200TC is a Series S01, yes. It could be field converted to a 200A main breaker device by installing a QOM2200VH Main Breaker Kit. If is a Series 001 or 002, no.

CTA-ID : 2050264
Was this helpful?
What can we do to improve the information ?