Technical FAQs

Ask a Question

What is the part number for an interior deadfront trim for a CQRA200?

Dead Front Interior Trim - 7329420101 (Also requires insulator and rivets, below)
Dead Front Interior Trim Insulator - 4053435601 (Attaches to rear of interior trim)
Dead Front Interior Trim Insulator Rivets - (2) 2430313230
Dead Front Interior Trim Mounting Screw - 4020513001K ( This kit contains 10 screws, but only one screw is required to secure the trim)



CTA-ID : 2050078
Was this helpful?
What can we do to improve the information ?