Technical FAQs

Ask a Question

Is the part number ZBY8330, 90 mm`` EMERGENCY STOP`` circular legend, available in French?

Issue:
What is the part number for a 90 mm emergency stop circular legend, in French? 

Product Line: 
22 mm operators XB4 / XB5

Environment:
North American Products

Cause:
​Would like a French emergency stop legend

Resolution:

It is available as part number ZBY8130. It is marked ``ARRET D`URGENCE``.
 
Was this helpful?
What can we do to improve the information ?