Technical FAQs

Ask a Question

Can the 52 circuit HOMELINE load centers be used in every state of the USA?

These load centers can only be used in states that have adopted the 2008 National Electrical Code or where the local inspection authority, or Authority Having Jurisdiction (AHJ), allows its use.


CTA-ID : 2049950
Was this helpful?
What can we do to improve the information ?