Technical FAQs

Ask a Question

What are the wind requirements of ANSI/IEEE and IEC?

ANSI/IEEE wind requirement is 90-100 mph.
IEC wind requirement is 75-80 mph.


CTA-ID : 2049928
Was this helpful?
What can we do to improve the information ?