Technical FAQs

Ask a Question

Which S-Flex units gets the top arc deflector shield?

208 and 230V Size A (1-10HP) and Size C (30HP)

These are the only units that receive the top shields.


CTA-ID : 2050829
Was this helpful?
What can we do to improve the information ?