Technical FAQs

Ask a Question

Are there instructions available for a 9065 bimetallic overload relay for NEMA sizes 00 through 2 and 5 through 7 ?

There are no instruction bulletins available for this device. There is a manual / auto reset selector switch. The overload requires requires 3 thermal units to operate and is a thermo-mechanical device.

CTA-ID : 2050826
Was this helpful?
What can we do to improve the information ?