Technical FAQs

Ask a Question

Is a space heater and thermostat available for I-Line, NF and NQ panelboards? Panelboard is to be used in a very cold environment.


Issue:
Is a space heater and thermostat available for I-Line, NF and NQ panelboards?   Panelboard is to be used in a very cold environment.

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product availability.

Resolution:
Yes.  Refer to NF panelboard section of current Digest                
These are available for top feed panels only, and panels must be factory assembled.  They are not available as field installable options.


CTA-ID : 2049985
Was this helpful?
What can we do to improve the information ?