Technical FAQs

Ask a Question

What is the difference between the LA400S and the LA400LS circuit breaker enclosures?

The LA400LS is physically smaller than the LA400S and has application limitations. The LA4000LS is UL listed only to accept a LAL, 3-Pole circuit breaker. The voltage is limited to 480Vac maximum. The SCCR is limited to 30K rms symmetrical amperes at 480Vac maximum. Copper conductors must be used (aluminum conductors are not acceptable).


CTA-ID : 2050780
Was this helpful?
What can we do to improve the information ?