Technical FAQs

Ask a Question

What component parts are supplied with the Class 9421 Type LZL250C46 through the door circuit breaker operating mechanism?

Product is supplied with the following:
(1) 9421LZ250 operating mechanism or saddle assembly.
(1) 9421LS13 long operating shaft with support bracket.
(1) 9421LC46 NEMA 3, 4/4X 6 inch chrome plated operating handle.

CTA-ID : 2050719
Was this helpful?
What can we do to improve the information ?