Technical FAQs

Ask a Question

9013FSG2: If the switch is not working properly what are some the things to check for?

If using switch with hard water make sure there is no sediment buildup in the switch and pipe, as this would cause a restriction. Sediment build up must be cleaned before switch will operate properly. Also, make sure the bladder is set 2 psi below the cut-in of the switch and that the bladder doesn`t have water in it. Lastly, check the check valve to see if it is working properly.


CTA-ID : 2050806
Was this helpful?
What can we do to improve the information ?