Technical FAQs

Ask a Question

Can a S29370, S29371 or S37422 be used on a Powerpact H or J breaker in a JD250S circuit breaker enclosure?

None of these accessories are suitable for use with the JD250S enclosure. A padlock hasp to lock the breaker in the OFF position is provided as an integral feature on the enclosure cover.


CTA-ID : 2050791
Was this helpful?
What can we do to improve the information ?