Technical FAQs

Ask a Question

Can the circuit breaker handle, when used in a HD100S circuit breaker enclosure, be padlocked in the ON and/or OFF position?

The cover of this circuit breaker enclosure has a weld bracket that functions as both a LOCK-OFF and LOCK-ON device for the circuit breaker when used with a padlock.

CTA-ID : 2050790
Was this helpful?
What can we do to improve the information ?