Technical FAQs

Ask a Question

Does the GS1GU3 meet MFPA 79 applications?

Yes, with the addition of the internally mounted GS1AD020 handle it will meet the NFPA 79 requirements.


CTA-ID : 2050724
Was this helpful?
What can we do to improve the information ?