Technical FAQs

Ask a Question

What type screwdriver is used to remove an AL400LA lug?

Torx head type T40 is the tool used to remove the mounting screw.


CTA-ID : 2050673
Was this helpful?
What can we do to improve the information ?