Technical FAQs

Ask a Question

What is the torque requirement for the wire binding screws on a HU361RB safety switch.

For wire sizes #14-#10 AWG the torque requirement is 35 in lbs; #8 AWG is 40 in lbs; #6 AWG is 45 in lbs.


CTA-ID : 2050618
Was this helpful?
What can we do to improve the information ?