Technical FAQs

Ask a Question

What is the part number for a 30mm pushbutton with push-on push-off operation?

Use a standard 9001 Type K momentary operator and the 9001 K85 push-on push-off module. This module will hold contacts depressed until button is depressed again. It is suggested to use a 9001KA4 or 9001KA6 for a NO contact.

CTA-ID : 2049924
Was this helpful?
What can we do to improve the information ?