Technical FAQs

Ask a Question

What is the torque requirement for the wire binding screws on a D222NRB safety switch.

For wire sizes #14-#10 AWG the torque requirement is 35 in lbs; #8-#4 AWG is 45 in lbs; #3 AWG is 50 in lbs.



CTA-ID : 2050647
Was this helpful?
What can we do to improve the information ?