Technical FAQs

Ask a Question

AP<br />Has some TECHNICAL_QUESTIONs on the base channels and lifting angles. Wanting to know if these can be removed.

Told him that yes but it is our recommendation that the base channels stay on for the support of the structure and the lifting would be find since it was for the lifting and moving of the structure.


CTA-ID : 2050745
Was this helpful?
What can we do to improve the information ?