Technical FAQs

Ask a Question

Is a UFP222R rated for load break?

Yes. If a device is horsepower rated it is a load make, load break device.


CTA-ID : 2050418
Was this helpful?
What can we do to improve the information ?