Technical FAQs

Ask a Question

Will the MP22125 accept the Lug Landing Kit #: MMSK2

No, the MMSK2 is suitable for use in 3-Gang through 6-Gang 125A maximum per position and 200A maximum per position MP, MPR and MPH style units.
Each MMSK2 is rated 600A maximum and includes (2) 1/2``-13 studs and mounting hardware.


CTA-ID : 2050298
Was this helpful?
What can we do to improve the information ?