Technical FAQs

Ask a Question

Is there a key interlock for a 9422CMP type operating mechanisms? Customer wants to interlock two breakers, in which only one at a time can be in the ON position.<br /><br />

No. There is no way to interlock two breakers and use operating mechanisms. Use of Interlocks and Operating Mechanisms are mutually exclusive.




CTA-ID : 2050296
Was this helpful?
What can we do to improve the information ?