Technical FAQs

Ask a Question

What is the lug size on a HU363DSWC and are there double lugs for it?

The lug takes (1) # 12 - # 1/0 (Al) or (1) # 14 - # 1/0 (Cu). There are no double lugs available for this switch.


CTA-ID : 2050310
Was this helpful?
What can we do to improve the information ?