Technical FAQs

Ask a Question

Where is the neutral terminated on a US21215018 mounting base?

This mounting base can use the second bus for the neutral. Then the neutral will be terminated on a the neutral pole of a 2-pole circuit breaker. It will be considered a switched neutral.


CTA-ID : 2050517
Was this helpful?
What can we do to improve the information ?