Technical FAQs

Ask a Question

Is there an alternate lug available for the DU325 safety switch?

Issue:
Lugs

Product Line:
General Duty Safety Switches

Environment:
Safety Switches

Cause:
Alternate lugs required

Resolution:
Yes, but for current design Series E03 only. Lug Kit GD4060LK, resticted to conductor combinations based on actual wire bending space provided in the switch, will provide terminals for (1) #1/0 AWG - 600 kcmil, (2) #1/0 AWG - 500 kcmil, or (4) #1/0 AWG - 250 kcmil, AL or CU conductors.

The kit consists of (3) line lugs, (3) load lugs and (2) neutral lugs, as required for a 3-pole, 4-wire, General Duty switch. Neutral lugs cannot be used on the DU325 switch.
Was this helpful?
What can we do to improve the information ?