Technical FAQs

Ask a Question

Since the FP222R has been obsoleted, what can be used instead for an air conditioning disconnect?

Consider using a QO24L70RB load center and a QO260 circuit breaker, or a QO2TR circuit breaker enclosure and a QO260 circuit breaker. The QO260 circuit breaker is HACR rated.


CTA-ID : 2050601
Was this helpful?
What can we do to improve the information ?