Technical FAQs

Ask a Question

Can a QO-HID breaker be used in a standard application as the QO breakers?

Yes, they can be used in standard applications and are physically interchangeable with the QO breakers.


CTA-ID : 2050339
Was this helpful?
What can we do to improve the information ?