Technical FAQs

Ask a Question

Do we have a replacement 200A fusible unit that is part of a 2 speed starter for Model 5?

Issue:
Do we have a replacement 200A fusible unit that is part of a 2 speed starter for Model 5?

Product Line:
Model 5 motor control centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The Model 5 mech assemblies are no longer available, but we use the same switch assembly and arc chute in Model 6 mech assemblies. They can order part # 8043983051 to get the Model 6 mech assy and take parts from it to use on the Model 5 mech.



CTA-ID : 2050178
Was this helpful?
What can we do to improve the information ?