Technical FAQs

Ask a Question

Can the 9001BW256 (ON-OFF Maintained) or any of the devices using contact symbol #10 be wired for a two wire control circuit?

Yes, just wire to the N.O. ON contact. When it is pushed it will close and remain closed until the OFF button is pushed when it will then open. (The N.C. off contact is never even used in this application).

CTA-ID : 2050678
Was this helpful?
What can we do to improve the information ?