Technical FAQs

Ask a Question

Can the ammeter trip indicator be removed or replaced in an SE breaker while the breaker is energized?

Yes , as long as the rating plug stays in. Installation must be done in accordance with working-hot procedures.


CTA-ID : 2050546
Was this helpful?
What can we do to improve the information ?