Technical FAQs

Ask a Question

What are the differences between the General Duty and Light Duty safety switches?

Product Features

Product Line:
Safety Switches

Product feature differences

In some cases the fuse types, The AIC rating capabilities, duty applications, Light duty is available in Nema 1 only and General Duty is available in Nema 1 or Nema 3R enclosures, and the General duty is supplied with spring activated quick-make, quick-break operating mechanicsms and the light duty is not.

CTA-ID : 2050382
Was this helpful?
What can we do to improve the information ?