Technical FAQs

Ask a Question

What Class of fuse does the T327N safety switch accept?

Issue:
Product design features

Product Line:
General Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:
This switch accepts 300Vac, Class T fuses ONLY. With Class T fuses installed, the switch is UL listed for use on systems with up to 100,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 2050244
Was this helpful?
What can we do to improve the information ?