Technical FAQs

Ask a Question

Are the handles provided on the covers of EZM Main Devices field replaceable?

Yes, two handles are typically used per cover provided on EZM Mains. Each cover is supplied with (2) 2940101103 handles that require (4) 2430315290 closed end pop rivets per handle.


CTA-ID : 2050231
Was this helpful?
What can we do to improve the information ?