Technical FAQs

Ask a Question

Does the XACA0* come with the hole in the bottom open or plugged?

The hole in the bottom of the XACA enclosure comes closed up with a knockout. It has a groove around it so that if you need to use it, you just remove the knockout. Only the holes in the cover are open.

CTA-ID : 2050166
Was this helpful?
What can we do to improve the information ?