Technical FAQs

Ask a Question

Can a 600amp Class L fuse be installed in a 800Amp Heavy Duty Safety Switch (like a H327NR)?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Fuses

Cause:
Application

Resolution:
The 800amp HDSS are designed to accept the 800amp Frame (601 - 800A) Class L fuses. If the fuse manufacture makes a 600A Frame Class L fuse that is physicallly the same size as the 800amp Frame, it will physically fit. However, BEFORE installing, please refer to your local electrical code authority to determine their acceptance.


CTA-ID : 2049248
Was this helpful?
What can we do to improve the information ?