Technical FAQs

Ask a Question

In MP Meter-Pak (125A maximum) meter centers and EZ Meter-Pak (125A maximum) branch units, what is the lowest 2-Pole Tenant Circuit Breaker ampere rating allowable?

Issue:
Product design features

Product Line:
Meter Pak and EZ Metering equipment

Environment:
Tenant breakers

Cause:
Application

Resolution:
The MP Meter-Pak (125A maximum) meter centers are not limited to a minimum amperage, they are only limited to a maximum amperage of 125amp max, 2-Pole Tenant Circuit Breaker position. See either the 2D CAD drawing for the specific catalog number or the wiring diagram on the device.

The EZ Meter-Pak (125A maximum) branch units are not limited to a minimum amperage, they are only limited to a maximum amperage of 125amp max., 2-Pole Tenant Circuit Breaker position. See either the 2D CAD drawing for the specific catalog number or the wiring diagram on the device.


CTA-ID : 2049466
Was this helpful?
What can we do to improve the information ?