Technical FAQs

Ask a Question

What is the heat loss contribution of a standard capacitor trip unit?

Once the capacitor trip unit has been charged, there is only a small trickle current to keep it at full charge. The current is so small that it can be ignored as a source of heat.


CTA-ID : 2049599
Was this helpful?
What can we do to improve the information ?