Technical FAQs

Ask a Question

Can the EZM 400A branch devices be ordered without the tenant breaker and then add it in the future?

Issue:
Supplied Tenant breakers

Product Line:
EZM Metering

Environment:
Factory supplied tenant breakers

Cause:
Requesting device less tenant breakers

Resolution:
No. The tenant breakers must be supplied from the factory with the meter unit.


CTA-ID : 2049247
Was this helpful?
What can we do to improve the information ?