Technical FAQs

Ask a Question

Is there an optional lug kit for the 200 ampere, Series F, Heavy Duty Safety Switches that will accept (2) conductors per phase?


Product Line:
HD Safety Switch

Selection of an alternate lug

Yes. The AL20DTF lug will accomodate (2) #6-250 Cu/Al conductors. The kit contains 3 lugs. However, the AL20DTF is not a UL Listed component and will not be noted on the switch's wiring diagram as an acceptable accessory. 

CTA-ID : 2049232
Was this helpful?
What can we do to improve the information ?