Technical FAQs

Ask a Question

Will the Power fuse be supplied on a Altistart48.

If the Altistat is ordered as a circuit breaker unit and the unit requires fusing for short circuit current ratings we will supply the power fuse. If the unit is ordered as a fusible unit we will not supply the fuse as standard.

CTA-ID : 2049367
Was this helpful?
What can we do to improve the information ?