Technical FAQs

Ask a Question

Is there a lug barrier available for a GS1GU3, making it able to comply with UL508?

The lugs on a GS1GU3 are recessed enough to comply with UL508 as well as UL98. No additional barrier is necessary.


CTA-ID : 2049594
Was this helpful?
What can we do to improve the information ?