Technical FAQs

Ask a Question

With the DPN Vigi breakers being obsoleted, what are the replacements?

Old part number for DPN-N Vigi 30mA in first column; replacement in second:

19661 6A C Curve 1P+N DPN Vigi (21555+21681)
19663 10A C Curve 1P+N DPN Vigi (21556+21681)
19665 16A C Curve 1P+N DPN Vigi (21557+21681)
19666 20A C Curve 1P+N DPN Vigi (21558+21681)
19667 25A C Curve 1P+N DPN Vigi (21559+21681)
19668 32A C Curve 1P+N DPN Vigi (21560+21683)
19669 40A C Curve 1P+N DPN Vigi (21561+21683)
DPN-N Vigi 300mA
19685 16A C Curve 1P+N DPN Vigi (21557+21682)
Was this helpful?
What can we do to improve the information ?